This positioning unit uses a readychain system to reliably guide drive, measuring system, and compressed air lines – 24 hours a day, seven days a week.
Mingseal uses our e-skin corrugated tube in its adhesive dispenser for camera modules. It combines the engineers' requirements regarding openability, inherent rigidity and compactness combined with the highest cleanroom suitability according to ISO Class 1.
A clean bottling, which does not have to be sterile, but has to be very clean, and a low overall weight of the system
Precise, reliable cleanroom 3D printer for processing thermoplastics.
As the quality requirements for cleanroom technology applications are constantly growing, igus® is continuously working on improving its products. For this purpose, igus® has been carrying out tests for cleanroom suitability in its own test laboratory since 1997. In addition, appropriate products are tested externally by the Fraunhofer Institute.
The cleanroom suitability of our iglidur® plain bearings is determined on the basis of the wear particles released in the application. The size and quantity of the released wear particles depend on:
• the respective pairing of shaft and bearing material
• further parameters such as load, speed etc.
Therefore, there are no clearly defined cleanroom materials for our plain bearings, but instead they depend on their use.