Motion plastics for the hydro energy industry

Machine parts that are used for generating energy via hydropower are exposed to extreme environmental conditions: they have to withstand very high loads, be resistant to saltwater and UV radiation and continuously operate without failure. Downtime due to material wear and frequent maintenance measures can negatively affect the energy output. igus® offers a large variety of customer-specific solutions that fulfil the requirements of these sources of renewable energy, and help improve the technology of the entire system. Whether wave power plants, hydropower turbines or screening plants - there are a lot of application areas for our plain and spherical bearings lead screws and energy guide systems in the hydro energy industry.
Would you like more information about products used in hydro energy? Our experts will be happy to get in touch with you.
 
Contact an expert
hydro energy

Maintenance-free products for use in hydro energy plants

igubal spherical bearings KBRM

Rod end bearings

Specifically for adjusting the rotor blades of hydropower turbines
  • Suitable for use in humid or wet environments 
  • Extremely low coefficient of friction in dry operation and very low stick-slip tendency
  • Find out more
Visit the shop
iglidur plain bearings UW

Plain bearing UW

For use in point absorbers
  • Extremely wear-resistant under water, tested and maintenance-free
  • For fast and constant rotation
  • Long service life
  • Find out more
Visit the shop
iglidur plain bearings TX1

igutex® bearings

Also suitable for underwater use
  • Heavy-duty bearings for loads up to 200 MPa
  • Wear-resistant and dimensionally stable
  • Good media resistance
  • Specially wound material
  • Find out more
Visit the shop
basic flizz complete system

basic flizz system

Complete system for the moving energy supply in screening plants
  • Low-maintenance, for travels up to 100m
  • Protection against weather and dirt exposure
  • Cost-effective and fully enclosed system
  • Find out more
Visit the shop
drylin high helix lead screws

High helix lead screws

Higher efficiency for the energy generator specifically in point absorbers 
  • Quiet and vibration-dampening due to rounded tooth geometry
  • Longer service life due to asymmetry
  • Find out more
Visit the shop
E4.1 e-chain

E4.1 e-chain®

Energy chain for wave energy converter
  • Tough, low-noise, modular
  • Hinged lids for fast insertion of cables from both sides
  • Cable-friendly interior separation 
  • Find out more
Visit the shop

hydro power

Benefits of igus® products in the hydro energy industry

 

  • Suitable for underwater applications
  • Resistant to dirt, dust and UV radiation
  • Lubrication-free and maintenance-free for 24/7 use
  • Extremely low coefficient of friction due to tribo-optimised polymers
  • For confined installation spaces and where there is very little room for movement
  • Low noise and low vibration
  • Long predictable service life
  • Low cost
  • Customised solutions from prototype to high-volume production
  • Large and varied range of products
  • Help from a specialist

Frequently asked questions regarding Hydro energy

What is hydro energy?

Hydro energy is a specific form of energy drawn from the power of water or hydro. It is the force of the water that creates the motion and therefore creates the power.

What are the advantages of hydro energy?

One of the key advantages of hydro energy is the fact it is a sustainable source of energy. As the energy is created from the water cycle, which as we all know is fuelled by the sun, it is a clean energy source and therefore renewable.

What are the disadvantages of hydro energy?

Like everything there are a few disadvantages such as limited amounts of water at certain points in the year, it can be a more expensive energy source and we are limited to where these hydro energy plants can be located.

For more FAQ's

Successfully in use

Further applications

Screening plant, rake cleaner

In order for hydropower plants to produce electricity reliably, the flow of water to the turbine must be guaranteed at all times. Any floating debris that collects on the protective screens of the water supply must therefore be removed regularly. This task is performed by screen cleaning systems, for example mobile horizontal/crosswise cleaners. As an alternative to trailing cables/festoons and busbar systems, we offer low-maintenance energy chain systems to reliably supply the travelling carriage with energy, in particular the basic flizz system, our standard for rake cleaners and scrapers.
Screening plant/rake cleaner
Screening plant and basic flizz

basic flizz energy supply system

  • Cost-effective complete system consisting of energy chain, chainflex cables and stainless steel housing
  • Protection against weather and dirt exposure
  • Low-maintenance, for travels up to 100m
Find out more about basic flizz

Water turbines

In Kaplan and Francis turbines, the water flow to the rotor blades and thus the turbine output can be regulated with the aid of adjustable, pivoting guide vanes. The adjustment mechanism consists of adjustment rings on the outside of the housing, which act on the rotary axes of the guide vanes via articulated levers. We offer the right plain bearings and rod ends for this purpose, which are robust, maintenance-free and corrosion-free.
Water turbine
Turbine detail, igubal KBRM, iglidur G plain bearing

Plain and spherical bearings

  • Lubrication-free flanged bushings made of the all-round material iglidur G or iglidur H especially for underwater applications
  • Rod ends igubal KBRM: corrosion-free, suitable for liquid media, with robust, long fibre-reinforced polymer spherical ball

Wave energy converter


Point absorber

Buoys anchored to the seabed with an integrated generator that converts the kinetic energy into electrical energy as the waves move up and down: point absorbers are considered a particularly promising wave energy converter technology. To guide the movement of the floating body and stabilise it even under adverse conditions, robust, maintenance-free linear guides are required, which we offer alongside sliding plates and compact, lightweight energy chains for safe cable guidance.
Point absorbers
Point absorber detail, igus products

Bearing technology and e-chain

Oscillating wave converters

An OWSC (Oscillating Wave Surge Converter) utilises the amplified liquid particle movement of waves in the near-shore zone. The conversion principle is based on a horizontal (more rarely vertical) pendulum movement of a flap that drives a high-pressure fluid in a secondary hydraulic system by means of a piston. We have the right plain bearings for the outer bearing points and for guiding the piston - high-strength, media-resistant and, as always, lubrication-free and maintenance-free.
Oscillating water columns
Oscillating water column, plain bearings TX1, TX2, H370

Plain bearings

  • For guiding the piston:
    Sleeve bearings iglidur H370 for high loads, with very good wear resistance under water
  • For fixing the water column and the main pivoting movement:
    High-strength wound slide bearings igutex X1 or igutex TX2, very wear-resistant under extreme loads
Oscillating water columns
Oscillating water column, plain bearings iglidur TX1, TX2, Q

Plain bearings

  • For guidance of the piston:
    Sleeve bearings iglidur Q for high loads, wear-resistant on many shafts
  • For supporting the main axis:
    High-strength wound slide bearings igutex X1 or igutex TX2, very wear-resistant under extreme loads

Seawater pump

The wave energy converter (WEC) "Searaser" is a pump consisting of two floats arranged one above the other and connected by a piston. As the waves rise and fall, seawater is pumped to a higher level on land so that it can be stored in large ponds and generate electricity with a turbine and generator when required. To guide the pump piston, we offer suitable plain bearings with particularly high wear resistance for underwater applications.
Searaser
Searaser detail, igus products

Plain bearings

Cylindrical bushings iglidur UW: extremely wear-resistant underwater endurance runner, the first choice for pump applications

Attenuator

This is another way to generate electricity from wave movements: with a long, modular series of floats connected via lever arms to a chain of electric generators. Placed in the direction of the waves, a serpentine movement is created as soon as the waves pass under the floats, and the levers drive the generators. We recommend our heavy-duty underwater plain bearings with flange for the many bearing points on both sides of the levers.
Attenuator
Attenuator detail, iglidur H370

Plain bearings

Flanged bearing iglidur H370 for high loads, with very good wear resistance under water


Consulting

I would be happy to answer your questions

Shipping and consultation

In person:

Monday to Friday from 8am - 8pm.

Online:

24h


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "RCYL", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus GmbH or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH