Solution
drylin ZLW toothed-belt axis in conveyor technologyThe persons responsible for mechanical design analysed the market and examined the solutions proposed by different suppliers. In the end, the multifunctional
drylin ZLW linear axis proposed by us convinced them (see Figs. 2 and 3 below). A good two metres long, 41 centimetres wide, 10 centimetres high and weighing 126 kilogrammes, it was supplied ready to install.
A total of four guide rails, two of which are used for parallel guidance, were assembled to create a compact system for KHS. This means that the three "thrust arms" (the middle one for sliding the kegs into the station, the two outer ones for moving them back onto the central conveyor belt) can be operated together on one shared linear axis.
To adapt the guide length of the carriages to the high torques that occur when the kegs are pushed across, the carriages are arranged on two levels. They are moved by means of two centrally located toothed belts (Fig. 4 below). As a space-saving measure, the motors are accommodated in the extension of the deflection axis on both sides of the unit.
iglidur plain bearings on the axesOn all axes,
plain bearings made of iglidur materials that need no external lubrication are used – an important aspect with regard to cleaning and filling under hygienic conditions. Moreover, an intelligently designed and easy to remove axial locating spigot enables fast replacement of the linear guide liners (Fig. 5 below).
drylin linear bearings in the lifting stationsIn addition, linear bearings are used in many places in the Innokeg AF-C Transversal. The axes of the lifting stations, for example, are equipped with
drylin stainless steel linear bearings (Fig. 6).
Condition monitoring for the plain bearing systemsFor the near future, the use of
isense technology to monitor the wear of the plain bearing systems within the framework of predictive maintenance is being considered at KHS. This can enhance the availability of the systems and increase the benefits to the customer.