Telescopic triflex® TRX- energy chain and retraction system in one

The TRX complements the functions of the triflex® R series and now also makes them telescopic

  • Due to their patented design, the chain links of the TRX allow a length compensation of up to 36% to one another without losing the connection or the torsional ability.
  • The rubber band inside the TRX retracts the links back to their starting point and the retraction force can be adjusted via the rubber band 
  • Weight reduction of up to 83% compared to a solution with a retraction system (RSP)
  • The TRX design study is currently 100% compatible with the TRE.60.087.0.B, other chain sizes will follow.
Would you like more information about our TRX? Our experts will be happy to get in touch with you.
Contact an expert

Experience the TRX from completely new angles

Start animation with the Play button and change the viewing angle with the mouse


Cable guidance in the TRX

As cables or hoses cannot be elongated to the same extent as the e-chain, they are placed in the TRX according to a specific principle. (see picture on the right) In addition, the cables and hoses are fastened in place in the middle of the TRX so that they do not leave their position when the chain is pulled. 
Thanks to the special arrangement of the cables/hoses, as well as the additional tension relief system in the centre of the TRX, the cables/hoses can cope with the length compensation of the e-chain® without any problems. 
 
Upper chain: cables/hoses wound onto a reel as much as possible
Middle chain: cables/hoses half unwound from reel
Lower chain: cables/hoses are completely elongated in the TRX
Transparent TRX with cables

The proof

The triflex® R TRX in the igus® test laboratory

The TRX is in its final testing phase in our in-house test laboratory at the moment. The picture shows the TRE.60.B size, in which the TRX will be available first. 
The first 7-8 chain links (starting from axis 6) are normal links of TRE.60.087.0.B. The rest of the e-chain is made of the new telescopic TRX e-chain.

Would you like to see it live? Just make a virtual appointment for our digital exhibition.  
Receive updates on the TRX

Suitable products for the TRX


The universal installation kit is ideal for attaching the TRX.
The TRX can be fixed in place with the supplied mounting brackets in different positions and can be supplemented with the suitable triflex® R chain up to axis 6.  

If you want more details on the easiest and quicket way to attach a fibre rod, click on the button below. 
Universal assembly kit
Universal assembly set_disassembled Including variably installable mounting plate for installing directly on the robot (dimension A, B, C)

Further products and options for the TRX

chainflex® robot cables

Find out more

TRX as readychain®

Find out more

readycable® robot cables

Find out more
robot cable management

triflex® R overview

Find out more