Solution
Our
iglidur plain bearings could help in many ways. Based on a lengthy consultation at Motek 2006, the entire bearing positions of the simulator were fitted with the plastic plain bearings. The decisive factor for the decision in favour of the bearings made of the material iglidur was that they are maintenance-free, cost-effective and very easy to handle. The installation took only seconds and no special bearing seats had to be constructed. In addition, enormous axial loads are also possible with the bearings. And should the wear be too high, the components can be replaced within a very short time. In addition to the plain bearings, our
plastic energy chains brought order to the cable tangle created by the complex electronic control system. The cables could thus be bundled without losing flexibility, which was an elementary requirement due to the rotation of the simulator.