Solution
Height and format adjustments:For various height adjustments,
drylin trapezoidal threads in combination with flange nuts made of high-performance polymers are used (see picture 1 below). The format adjustments are made via drylin R flange bearings (picture 2).
Electric motor bracket:The
igubal clip bearings are installed on the bracket of an electric motor to ensure easy installation (picture 3).
Vertical linear axis:On another (vertical) linear axis, Küppersbusch has been using a combination of
drylin R fixed flange bearings with aluminium adapters in which anodised aluminium shafts move for many years (picture 4). It does not need any lubrication and is almost wear-free.
Rotary table outlet and bottle feed:The outlet of the rotary table, when feeding the bottles, was originally made of stainless steel. In order to dampen the noise of bottles hitting metal, tribo-tape made of iglidur B160 is used at present (picture 5). The liner is resistant to cleaning agents and is characterised by a very good coefficient of sliding / friction compared to glass.
Filling and dosing stations:At the valves and pumps of the filling and dosing stations, the bottles are
drylin T rail guides and connected to the filler. At the centring bridges of the filling tubes, the company installs
iglidur flange bearings (picture 6), which are not only FDA-compliant and chemically resistant, but also have an extremely long service life.