Solution
For this reason, drylin linear bearings in particular, but also plastic plain bearings made of iglidur are used at various points within the testing and packaging system.
For side and format adjustments to set the machine for different folding box dimensions,
drylin SHT linear systems are used, which can be adjusted precisely by hand (see picture 1 down). The
drylin lead screws used are robust and allow adjustments under high loads and long stroke lengths (picture 3).
A highly wear-resistant
round bar made of iglidur JB is used as a transfer roller in the system. It also offers low coefficients of friction and operates without lubrication (picture 2).
Several pressure rollers are used for product transport, which keep the products securely on track and ensure the short processing cycles. In the rollers, lubrication and maintenance-free
plain bearings made of iglidur J prove themselves in continuous operation (picture 4).
In addition to the format adjustments of the testing and packaging unit,
drylin SHT lead screw linear systems are also used for the adjustment of the sensors. Their precision and robustness guarantee convenient operation with maximum availability (picture 5).
Last but not least, Wipotec's module also uses
xiros ball bearings in the guide rollers. Like all components, they are also fully FDA-compliant (picture 6).