Solution
The project management of the technology department at Wiegel Verwaltung GmbH & Co KG decided at this point in favour of
polymer energy chains from our product portfolio, which offered the customer two advantages above all: a tight-sealing solution for the area of material preparation, which was previously not the case with a festoon system, as well as high wear resistance.
The first energy chain was used in a Wiegel plant in 2015. The next application followed a year later, where we supplied both the
E4/4 series energy chain and the new
plastic trough made of the chemical-resistant material igumid EG+. This ensures a high resistance to chemicals, so that the use of the guide trough is ideal for use in hot dip galvanizing or, for example, fertiliser production. The igumid EG+ is characterised by very low water absorption. This offers increased resistance to aggressive chemicals. The material can be used in a temperature range of 0 °C to +100 °C with its clearly optimised sliding properties for the guide trough and also for most series of e-chains. Since both the e-chain and the trough in the complete system consist of the chemically resistant material, they are very good gliding partners.