Single Pair Ethernet (SPE) - now also for the e-chain with a 4-year guarantee


What is Single Pair Ethernet?

Single Pair Ethernet technically describes the transmission of Ethernet (1000Base-T1) via only two pair of copper wires and enables both data transmission via Ethernet and simultaneous power supply (PoDL). This technological leap leads to a reduction of the diameter by approx. 25% compared to an ordinary Ethernet cable.

Single Pair Ethernet technology (SPE) is the key to smart industrial automation, the Industrial Internet of Things (IIoT). For the first time, this enables uniform, space and cost-efficient Ethernet communication, including the "last metre" from the cloud via the switch cabinet to the machine. 

Would you like more information about SPE cables or do you need an individual consultation? Our experts will be happy to get in touch with you.

Contact an expert



single pair ethernet cable

How can SPE be used now?

The significantly increased transmission rate with simultaneous reduction of the diameter will also allow  the cost-effective connection of sensors with high data volumes in the future. The user doesn't have to forego quality in the process. The oil-resistant and flame-retardant CFBUS.PUR.042 has been extensively tested in the 3,800m2 igus test laboratory . As with all chainflex cable ranges, for the Single Pair Ethernet cables, the customer will also receive a guarantee of 10 million double strokes or 48 months.
 
SPE is therefore a real alternative to other bus systems in applications with small bend radii and small installation spaces, such as industrial camera applications or position or monitoring sensors.  Such camera vision systems primarily serve as detection and positioning systems.  Until now, such sensors had to be connected in the field via bus interfaces with 4 or 8-core Ethernet cable. With SPE, each sensor can be directly integrated into the superordinate control level.

Single pair ethernet cable applications


Who is driving the new SPE technology?

The SPE Industrial Partner Network

Single Pair Ethernet is the infrastructure foundation that makes IIoT and Industry 4.0 possible. In order to promote Single Pair Ethernet technology for the rapidly growing IIoT market, igus is participating in the SPE Industrial Partner Networks with other strong partners such as HARTING or TE Connectivity.  
 
For the reliable establishment of the entire future SPE ecosystem, standards for transmission protocols, cabling and device components are also jointly developed and adopted and published in IEEE 802.3 and IEC SC46C.  
 
In this way, the new cable could also be constructed in partnership for the T1 connector interface. As a result, the durable shield has reliable transference to the connector, ensuring optimal high electromagnetic compatibility (EMC). The combination of chainflex cable and SPE connector is extremely robust: igus uses a highly abrasion-resistant and notch-resistant PUR jacket, and the connector has tough metal latches with a PCB socket.
 
Find out more

Are you looking for an chain for your cable?

Find your e-chain®
readychain

.....or do you require a fully harnessed version?

To the readychain