SCARA cable solution

Durable energy supply on the SCARA robot


igus® has developed the e-rib to safely guide cables guided by corrugated hose. In combination with the reinforcements at both ends of the corrugated hose as well as the rotary unions, this solution is ideally suited for high-speed SCARA applications.
 
The e-rib fills the joints of the corrugated hose to stabilise it in such a way that it can only move in one direction. The corrugated hose has an unsupported length due to the lateral guide elements. As a retrofit, the e-rib allows an upgrade of existing applications in just a few steps. The e-rib is independent of the hose manufacturer. At first we are offering this solution in the nominal width of 29mm.

Did you know that you can have your e-rib recycled as
part of the igus® chainge Recycling Program at the end of its life cycle... 

Would you like more information about our scara products? Our experts will be happy to get in touch with you.
 
Contact an expert

Scara robot cable solutions

Corrugated tubes

scara robot
  • Corrugated reinforced tube for high speed applications
  • Fixed and moving end options available. 
Visit the shop

e-rib

e-rib
  • Can be easily retrofitted
  • Longer service life for cables in corrugated tubes
  • Available in four sizes
Visit the shop

Robot cable management

triflex
  • triflex® R cable management for multi-axis, industrial robots
  • Find out more
Visit the shop

Augmented reality for SCARA Cable Solution

Use augmented reality capabilities and project the EPSON T3 402S SCARA robot onto its future production site with the SCARA Cable Solution or just into the office to make planning even more realistic. 

Simply scan the QR code and use the 3D model and the augmented reality (AR) model with a tablet or smartphone. 
Start AR desktop version
Augmented reality SCARA Cable Solution Scan the QR code and try it yourself

What is behind the Scara cable solution?

Corrugated tube dynamically reinforced

The reinforcement for existing corrugated tube systems. The e-rib is clipped onto a corrugated hose. The new sizes are independent of the hose manufacturer. The e-rib stabilises the corrugated hose so that it can only move in one direction. With its lateral guide elements, the corrugated hose requires no support along its length due to the e-rib.
Initially we offer the nominal width 29 for the Scara robots. 
 

e-rib_1

Scara cable solution in the igus test laboratory


This video recorded at the igus® test laboratory shows how the SCARA cable solution works.

The ends of the SCARA mounted on ball bearings ensure an unrestricted rotary connection of the corrugated hose. The e-rib in conjunction with the corrugated hose provide stability so that the corrugated hose doesn't kink due to the movement. 

Example of the structure of part numbers:
SCARA EPSON G6 553s

The SCARA Cable Solution consists of three elements matching or adapted to the SCARA robot in question. 

1: Moving end attachment (straight): TR.SCS.29.01.20.94.01.0

2: Moving end attachment (angled): TR.SCS.29.01.20.94.02.0

3: Fixed end attachment: TR.SCS.29.02.40.01.0

4: Corrugated hose with e-rib: TR.SCS.29.LLLL.0
View Scara solutions in the online shop
Scara Cable Solution: end pieces and hose
cable solution scara

Clean SCARA cable solution

  • Suitable for cleanroom according to IPA certificate ISO Class 2
  • Safer guidance of cables and hoses in cleanroom
  • All components can be indivdually relaceable retrofitted
  • Rotary mounting
  • Over 2,000,000 test cycles have been carried out at the igus® cleanroom test laboratory
Download our cleanroom brochure 
​​​​​​​ 
Find out more

Frequently asked questions

What is a Scara robot?

A scara robot is a robot arm for industrial robots, usually used in high speed applications.

What is a Scara robot cable solution?

This is a product added to Scara robots which guides cables safely.

What are the benefits of the igus® scara robot cable management?

Similarly to the triflex® robotic energy chain, the system used for the scara is a modular system ensuting easy to retrofit.

Read more FAQ's here

You might also be interested in this

chainflex® cables

chainflex® cables Dependable cables with an up to 36-month guarantee for moving applications.
Find out more

readychain® complete system

Harnessed energy chain systems Everything from a single source! Harnessing time decreases by up to 95%.
Find out more

energy chains

Robotics home page Overview of all plastic energy supply systems.
 
Find out more