A data cable is a multi-core cable used for simple transmission of data and information. It is important that the information moves securely from the sender to the receiver.
igus® data cables are used wherever large amounts of data must be safely transmitted in motion. They are usually shielded and carry a wide variety of application signals. Differently structured data cables are used for the simple transmission of information in industrial plant and machines. The information is converted into voltage or current signals, which are often designed as 0 to 10 V or 4 to 20 mA signals.A system that has to work around the clock under high pressure requires the highest standards - also from the suppliers of the individual components of the machine. An example of this would be the "Speedmounter" system from IPTE GmbH. By using our energy chains and chainflex data cables maintenance intervals have been reduced and the company can save considerable costs. In addition, our cables attract with their special design, with gusset-filled extruded inner jacket, they retain their transmission properties after many millions of double cycles.
A team of students at Karlsruhe University of Applied Sciences set themselves the goal of converting a kart with an internal combustion engine and road approval into an 'e-kart' that provides maximum driving pleasure. For years, the electric kart has been undergoing optimisation and conversion at the hands of the students. Until recently, a new fast-charge battery was integrated, and many of our products were also used. Among other things, shielded cables that withstand the high speeds and accelerations.