Solution
For the conception of the energy supply system, the drawing documentation was prepared and the approval protocol was made during commissioning. The performance design was always coordinated in close cooperation with the crane builder Kuenz. In the application case, the entire performance package consists of the provision of the energy supply system, the cables, the strain relief and the guide trough.
The RGB cranes are now each equipped with a pre-assembled
readychain energy supply system, or more precisely, a roller energy chain from igus is used here. There are no additional loads on the energy supply system, which runs in a
guide trough. "It only runs in the direction in which it is supposed to move," confirms Günter Baitis. Guide troughs are used for long travels. They facilitate smooth, low-friction operation of the energy supply system. For reasons of weight, among others, an aluminium material was chosen for the RGB cranes, which is also seawater-resistant according to DIN.
The roller energy chain is covered with chainflex special cables such as power and control cables. In addition to the quality of the cables used, the arrangement of the cables within the chain and the available space basically play a decisive role with regard to the service life of the system.