Problem
The fertiliser spreaders from RAUCH Landmaschinenfabrik GmbH, such as the model AXIS 50.1 W in this case, dose with the highest precision when spreading fertiliser evenly on the field. Here, all components used in the fertiliser spreader must be corrosion-free and designed for the high content of ammonia in the fertiliser. This is also the case in the boundary spreading device, which limits the spreading area of the fertiliser to enable more targeted and efficient spreading. Here, clevis joints are used in combination with a KMF hydraulic cylinder, which must be able to permanently withstand the adverse conditions.