The functionality of slewing ring ball bearings is based on an inner race, an outer race and a row of balls in between. These balls serve as rolling elements and enable a rotary movement between the rings. Thanks to their special design, slewing ring ball bearings are able to absorb high loads while minimising friction losses. This leads to an extremely efficient transmission of forces.
The advantages of slewing ring ball bearings are manifold. They primarily enable a rotary movement with minimal friction. This is particularly important in machines and systems where precision plays a decisive role. Secondly, slewing ring ball bearings can absorb large axial and radial loads, which is ideal for applications with high loads.
In addition, slewing ring ball bearings have a compact design and are lightweight, which saves space and optimises weight.
Ball bearing slewing rings can be used in a wide range of applications. In robotics, they are used in joints to perform precise movements and enable positioning. In aerospace engineering, they are used in swivelling tables and joints to align antennas, cameras and sensors. Slewing ring ball bearings are also used in medical technology in medical devices. Other areas of application include the packaging industry, semiconductor production, machine tools and many more.
When selecting slewing ring ball bearings, certain aspects should not be ignored. These include the required load capacity, the desired accuracy, the operating environment (such as temperature, corrosion and dust) as well as the installation and maintenance requirements. It is important to choose the right size and design of ball bearing slewing ring according to the specific requirements of the application. We can help you with this.