Solution
DST has been using
energy supply systems from igus for a number of years. In close cooperation with igus, the design engineers at Dörries Scharmann have developed a concept for connecting the energy supply system to the machine in such a way that, on the one hand, there are few interfaces and, on the other hand, a clean supply of all components is guaranteed. Another major concern was to make the assembly of the machining centres as simple and planned as possible, so that no problems would arise.
In concrete terms, the "DBF 630" machining centre is now equipped with two energy supply systems that are sold with ready-harnessed chainflex cables under the name
readycable. The ready-to-connect cables can be installed in a time-saving manner. From the actual energy supply system up to each chainflex special cable, the machine builder relied on high quality parts: All bus, servo or control cables are equipped with integrated strain relief elements. In addition, there are additional interior separation elements to increase the service life of the individual cables. Connectors, connections and steel components specified by the customer round off the complete pre-assembled system.
Since Dörries Scharmann manufactures exclusively to customer specifications, the difficulty lies in defining the exact length of the supply cables. Therefore, it was important for the machine specialist to have a supplier who could provide technical support, respond flexibly to the different requirements and, above all, implement the order at very short notice. Stefan Nethövel, Division Manager Materials Management/Logistics at Dörries Scharmann adds: "When the machine concept is established, the delivery of a completely pre-assembled energy supply system must be guaranteed within ten working days. “