Solution
Bihler's designers tested various energy supply systems. In combination with the chainflex cables, the
E2/000 energy chain from igus proved itself best. A closed version of the chain with an additional protective fabric hose is used in some places within the machine. This prevents stamping residues from getting into the chain. The energy chains in the upper and lower areas have zones with a reverse bend radius so that they can adapt themselves to any desired position and therefore save space. The cables used are [ chainflex servo cables of type CF270.UL.D and encoder cables of type CF113.027.D on the units and for the adjustment drive.
Bihler factory personnel require six energy chains per press, which are filled not only with the comparatively heavy servo cables and signal cables but also with hoses for cooling and lubricant. Each of the six chains has a different length and a defined configuration. And because Bihler wants to be just as fast and flexible in its own assembly as the users of the Bihler servo machines are in their work, igus supplies a set of six completely filled and assembled chains as "
readychains" in a readychain rack specially designed for this purpose.