Solution
The application head today features several plain bearing applications that absorb high forces and shocks. The bearings are found first in the pivot point for the pressure sensor system and second serve as roller bearings.
Specifically, these are
bearings from the iglidur G family, which weigh only little and have larger inner diameters than ball bearings. The economical all-rounders withstand extremely high loads and operate at low to medium surface speeds. The self-lubricating effect makes them maintenance-free in dry operation and insensitive to dust and dirt. As with all iglidur plain bearings, the high-performance material used is composed of base polymer, fibres and fillers as well as solid lubricants. These components ensure that the coefficient of friction and the specific coefficient of wear are set as low as possible. The iglidur G plain bearings also have a good resistance to chemicals. Most lubricants cannot harm them. The same applies to many weak organic and inorganic acids. In addition,
iglidur J plain bearings have a particularly low moisture absorption and low coefficients of friction. The specialist for fast and slow movements ensures very low friction values and the lowest stick-slip tendency in the "Innopack CSM". It is recommended for applications with medium compressive forces - at high speeds and high wear resistance.