Solution
The company used a combination of
drylin W single rails as linear bearings and flanged
iglidur Z plain bearings to address all issues and concerns.
The previous application's main problem was the steel linear technology. The linear plain bearings from the drylin range, operate without lubricants and require no maintenance at all. This not only makes them insensitive to the large amounts of dust in the plant, but also allows them to work with greater precision. As damage to the products is avoided, product quality is improved. The ball bearings from the iglidur range also operate without maintenance, eliminating the clearance of the previous steel bearings.