Solution
First, the project managers tried out stainless-steel rolling bearings. However, the contact between the metal ball bearing and the guide created noise on the carriage that exceeded the acceptable limits in hospital ambience. Furthermore, the friction caused by the movement put additional strain on the motor and thus the entire system. In addition, the steel bearings also failed the service life tests and achieved only 10-20% of the expected service life of the product.
Therefore, the engineers finally decided to support and move the devices into the UV chamber with our
drylin W linear guides, which operate completely free of lubrication and maintenance. This is achieved by the solid lubricants incorporated in the sliding elements. In this way, it was not only possible to fulfil the claim of being able to do without lubricants. This also ensured the continued reduction of noise in the cleaning device: due to the use of lubrication-free liners, and also because the bearings slide instead of roll, the steriliser now runs exceptionally quietly.
And two further advantages resulted from the use of drylin linear systems: they are not only insensitive to dirt and dust, but also represent a cost-effective and very flexible solution.