chainflex® cables for use in the offshore industry

chainflex® cables with "DNV" approval and NEK 606 MUD-resistant approval for maritime use

To allow cables to be used for moving applications on ships and offshore applications without the need for time-consuming and cost-intensive special approvals, igus GmbH and the DNV classification company developed a new test procedure. As a result, a total of 387 chainflex cables from igus have now received type approval for permanent movement in e-chains.
This makes them the first cables in the world specifically for applications in energy chains to receive this approval.
 
Contact an expert

Approvals & standards

The importance of the approvals & standards for chainflex cables

In challenging environments like offshore and marine applications, the reliability and durability of your cables is essential. This is where the MUD NEK 606 and DNV approvals and standards come into play.
These ensure your cables meet the best performance and safety requirements. 

Why are these standards and approvals so important? 
Both the NEK 606 MUD-resistant and DNV are available in most of our PUR jackets, which means this range of cable are equipped to handle the challenges of offshore applications. 
We also offer other cables which are DNV-GL approved in our TPE range. 

NEK 606 logo

MUD-resistant according to NEK606


The NEK 606 MUD-resistant standard is a Norwegian technical specification designed for the marine and offshore industry. It covers a range of cables that are MUD- resistant, meaning they can withstand exposure to hydrocarbon-laden drilling mud used in offshore drilling operations. 

This resistance is key because drilling mud can have detrimental effects on the cable, which could ultimately lead to cable failures and safety hazzards. 

Cables which comply with the NEK 606 standard are tested on their ability to last in harsh conditions with extended exposure to mud at high temperatures. 
 

DNV approvals

In order to supply safe and suitable products for these applications, igus worked with the DNV classification company to develop a new testing procedure and to have their chainflex cables certified.
The DNV is a globally recognised certification body that sets the standards for safety, quality and environmental sustainabilty in the offshore and marine industry. 
Cables that are DNV certified have gone through harsh and rigorous testing to ensure they meet the highest standards of safety and reliabilty. 
 
Development of new testing procedures necessary 
Classification companies such as DNV typically issue approvals that are in line with international standards. In many cases, particularly concerning the materials, these refer to special specifications with regard to fire behaviour or other requirements.
Over a long certification time of more than three years, with very different areas of investigation, the special knowledge of the two companies led to a cable designation for use in energy chains on ships and in offshore applications for the very first time.
DNV logo

Our chainflex® cables

CF77.UL Control cable

control cable
  • Cores wound in bundles for a long service life  
  • PUR unshielded control cable  
  • Large range of core cross section combinations 
Visit the shop

CF78.UL Control cable

Data cable
  • Cores wound in bundles for a long service life
  • PUR shielded control cable  
  • Large range of core cross section combinations  
Visit the shop

CF240.PUR Data cable

Bus cable
  • Wound in layer cable design  
  • PUR shielded data cable  
  • Best EMC properties due to high shield coverage
Visit the shop

CF211.PUR Data cable

Fibre optic cable
  • Twisted pair cable design 
  • PUR shielded data cable 
  • Best EMC properties due to high shield coverage 
   
Visit the shop

CF112 Data cable

Measuring system cables
  • Twisted pair with a pair shield 
  • PUR shielded data cable 
  • The highest EMC properties due to high shield coverage  
Visit the shop

CFBUS.PUR Bus cable

Servo cables
  • Simple selection matrix for a good overview 
  • PUR shielded cable following BUS protocols 
  • Reliable data transmission 
   
Visit the shop

CFLG.LB.PUR Fibre optic cable

Motor cables
  • For long distances and transmission of large data  
  • PUR outer jacket  
  • Several options of number of fibres and fibre size 
Visit the shop

CF111.D Measuring system cable

CF111.D
  • Electrical design according to manufacturer  
  • PUR shielded cable designed for <10 M
  • Halogen free and flame retardant
   
Visit the shop

CF113.D Measuring system cable

chainflex cable
  • Electrical design according to manufacturer  
  • PUR shielded cable designed for 100 M 
  • Halogen free and flame retardant  
    
Visit the shop

CF27.D Servo cable

chainflex cable
  • Various structures with one or two pair
  • Innovative shield pair structure  
  • Special core insulation for greater current flow 
Visit the shop

CF280.UL.H Hybrid cable

chainflex cable
  • Specifically designed for drive manufacturers 
  • Wide range of core configurations 
  • One cable technology  
Visit the shop

CFSPECIAL.532 Data cable

special532.3
  • Data cables for top drive  
  • Designed high tensile loads 
  • Optimised for oil and gas drilling applications 
Visit the shop

CFSPECIAL.572 Motor cable

special572.40.02
  • Motor cables for top drive  
  • Designed high tensile loads 
  • Optimised for oil and gas drilling applications 
Visit the shop

CFSPECIAL.592 Hybrid cable

special592
  • Hybrid cables for top drive  
  • Designed high tensile loads 
  • Optimised for oil and gas drilling applications 
Visit the shop

Visit the cable overview

chainflex overview
  • Still unsure on which cable works best for your application?  Use the cable configurator  or alternatively you can visit the chainflex overview
Visit the cable overview

You can find the right cable for your application

e-loop banner
To the chainflex product finder

Free white paper

Maritime whitepaper

More automation in the maritime sector

What challenges, what advantages do automotion and digitalisation bring to the maritime industry? How can companies meet the strict test criteria to have components certified by competent instituations such as DNV? What opportunities arise for suppliers, plant manufacturers and operators of drilling platforms and ships through the use of certified components such as cables? 
eloop whitepaper

Cable guidance under adverse conditions

Originally developed for a very sprecific application in deep drilling rigs, the e-loop energy supply system is also used in bucket wheel excavators, ship unloaders and in the construction of offshore wind turbines in just a short time after its market launch. In this white paper you will find various cases as a source of ideas. 

Energy chain options for offshore and marine

E4.1 series

E4

The energy chain designed for
virtually all applications

  • Tough
  • Modular system
  • High stability
E4 overview

E4.350 energy chain

E4.350

The worlds largest polymer energy chain

  • Extremely strong
  • Noise reducing
  • High push/oull strength
E4.350 example in drilling vessel

e-loop

e-loop

The igus® alternative to the service loop

  • High strength pull rope
  • Ideal for 3 dimensional applications
  • Perfect for drilling rigs
More information on the e-loop