Problem
Modular drilling rigs are required for such situations as when drilling equipment needs to be added to fixed drilling platforms.
Mobile drilling vessels have all the necessary equipment for mooring at the drilling station and precisely placing the extended drill pipe. For this purpose, a huge cantilever moves over the drilling platform over which the drill pipe is finally to be set up and precisely positioned. Large cable guidance systems are required to ensure that the entire movable structure for setting up and placing the equipment can also move smoothly and without failing. In this application, the cantilever should be able to travel 17.5m, the mobile drilling floor 8m. The moving cables reach an additional load of 200kg/m, a major cable guidance challenge. The harsh conditions at sea meant that the solution needed to be particularly robust and durable, withstand corrosion, and have as little dead weight as possible.