Solution
The disorderly pile of countless electrical and pneumatic cables could be bundled in a
triflex R energy supply system. The entire plant looks compact and clean today, even at first glance. Due to its round design, the energy supply system glides over the outer contour of the robot. It cannot get hooked and jammed in the process. Since the lattice box to be filled is not very large, this is an extremely important point. The energy chain guides the cables with a defined minimum bend radius. The bend radius is the same in all directions.
The triflex system shows its strengths wherever there are movements in more than two directions. These are primarily applications on 6-axis robots, which can be found, for example, in all environments on welding and painting applications, in gluing and grinding technology, but also in the assembly of gearboxes or in screw fastening processes. It is also used in the Scara robot at extremely high speeds. Fibre-rods can be integrated in the triflex R in order to integrate specific preloads. They give the energy supply system a certain alignment and keep it away from interfering edges. With conventional systems, it is partly done by elaborate springs, rope pulleys or guide systems. In addition to the increased space requirement and new interfering edges, these external elements exert further forces on the energy supply system - with all the resulting disadvantages.