Höfler Maschinenbau GmbH (now under Klingelnberg AG), a traditional company based in Ettlingen in Baden-Württemberg, specialises in the design of gear grinding and gear milling machines. For such a gear grinding machine, a special solution for the energy supply system had to be found for a customer due to the structural environmental conditions. A vertical stroke of 1320 mm and a pivoting range of the grinding head of 270° (-180° to +90°) had to be achieved in a rather limited installation space. An energy chain in a conventional hanging arrangement could not be accommodated in the given installation space.
In order to meet the specified requirements, the
energy chain system from igus was chosen as the fixed point at the bottom. The chain, which can move on both sides, is guided by a pivoting guide roller, which is connected to a counterweight by means of a toothed belt. This keeps the chain under tension at all times. In the meantime, the decision was made to install the energy chain in batch production due to the good experiences. The igus energy supply system has been used here for many years without any problems.