Solution
Since the commissioning of the composting plant, energy supply systems from igus in various lengths and designs have been in use in the layer rearrangement unit, the so-called Wendelin.
The Wendelin has a longitudinal chain and a transverse chain in the system. In addition, there are two more chains at the input for conveying and distributing the bio-waste in the first heap, making a total of eight energy supply systems in operation. Apart from the longitudinal travel, only 'rol e-chain' roller energy supply systems of the modular and robust
E4/4 system are used.
Roller energy chains display their full strength with long travels, high speeds as well as high cable loads.
In contrast to gliding e-chains, the necessary drive forces can be reduced by 75 %. The coarse and coarsest dirt particles especially on this unit usually lead to increased abrasion. In the evenly rolling operating mode, the rolling resistance and thus the wear of the chain are minimised. Their service life increases considerably.
Their service life increases considerably. In addition to the roller energy supply systems, chainflex cables,
guide troughs for the long travels as well as separators and strain relief elements from igus are also in use. The unshielded control cables 'chainflex CF 5' are located in the energy supply system. Due to its construction, with gusset-filling extruded inner jacket and the PVC outer jacket, the series is suitable for the highest stresses.