Encoder cables, or measuring system cables are required to transmit signals between position sensors of servo motors and their control systems in industrial plant and machines. These signals usually include, among other things, information about the position and speed of the machine.
The various signals generated by the angular encoder map the exact movement of the motor and are transmitted along with this movement. As a rule, not only the data of the encoder system is transported in the cable, but also the supply of the encoder is realised.