Solution
Muhr found this alternative in our
basic flizz system. It is a complete solution for energy supply to moving components in such systems as sewage treatment plants and energy and crane technology. The system consists of an energy chain from our
E4.1 modular system, which is filled with
chainflex cables and guides them safely in a weatherproof stainless steel enclosure. The advantages were obvious as soon as the first basic flizz was mounted on the rake cleaner in Rochlitz. While it normally took the fitters on site a day to install the energy supply system, they were able to complete the task in an hour and a half. And the cable trolley for the moving energy supply, which is about 15 metres long, required only 30 centimetres of installation space. This not only means more room but also saves cable length and copper.
Other advantages the Muhr engineers saw were the energy chain guidance system, which is protected on three and a half sides, and the freely suspended cable routing, which prevents cables from freezing in ice and snow. The basic flizz is mounted more or less invisibly behind the linear drive but is easily accessible if required. New cables can be added without any problems and there is no need to replace the entire cable package, as there is with a festoon system. This is why Muhr now only uses the basic flizz system for its H-series.
Two sensors measure water levels upstream and downstream of the rack and give the signal for the system's PLC to start the cleaning process. At a specified difference the PLC initiates the cleaning process that takes only seven minutes. The situation at the Rochlitz Schlossmühle rake is monitored by two cameras. This modern technology and the durable energy supply system will contribute to efficient hydroelectric power plant operation for many years.