The unit is mounted on the tractor and is therefore exposed to all weather conditions as well as sand and soil. There were three other problems for Thiessen Tillage to solve:
1. Movement takes place in the bearing points at low speed, but continuously.
2. The bearing points are radially loaded
3. The risk of failure due to insufficient lubrication
Initially, the company experimented with greased steel bushings and deep groove ball bearings. However, low-maintenance plain bearings were needed that can be used easily and cost-effectively and withstand the harsh environmental conditions. So the decision was made for iglidur® plain bearings.
By using iglidur plain bearings, Thiessen Tillage Equipment was able to dispense with the use of grease nipples at the bearing points. Also in terms of design, iglidur plain bearings offered advantages. Through your efforts, the design and size of the cultivation system could be adapted. For the end customer, they offer the advantage that they can be easily replaced in their own workshop if necessary.