Solution
The numerous cables, such as optical fibre or signal cables are now routed in the respective specifications in several
e-spool HD systems. This is an energy chain including a drum that can be rolled up and unrolled safely and in a space-saving manner.
The e-spool was used instead of a traditional cable drum, as the latter would have required the construction of special cables that would not have been tested in use and whose performance would have been unknown. With the e-spool, the wide cable mix can be handled in full compliance with the project requirements together with the multimedia technology.
The e-spool system was installed near the hydraulic winched in a machine room. From here, the energy chain is diverted to the devices via a specially designed guide and roller path.
Alfa System Sas also relies on our
chainflex product portfolio for moving applications for the cables themselves. Thanks to a wide range of products, the customer was able to find all the required cable specifications in one place. In addition, we offer a 36-month guarantee on all cables in the portfolio.