Solution
Our colleague Axel Ebert from Switzerland visited Rad9 with a bag of samples full of linear solutions. The technical requirements were defined on site, and it quickly became clear to the experienced igus application engineer that the drylin
® W modular system was just the thing. Together they decided on the
drylin® W double profile guides - two metres long and with a shaft diameter of 20 millimetres, with a guide spacing of 80 millimetres. The ten-millimetre rail would have sufficed, but the price difference was so minimal that the company opted for the more solid version due to its strength, durability and appearance. They also decided on four matching
drylin® W linear housings from the modular system. The
drylin® W double profile guides are made of hard-anodised aluminium and are therefore corrosion-free. The pillow blocks from the drylin
® W linear range are also designed for dry operation and use no lubricants, such as oils or greases. The drylin
® W linear product range has many advantages over conventional recirculating ball bearings. No lubrication is necessary, dirt and dust cannot adhere and there is no costly maintenance. MAX Velolift focused on reducing the lift to the essentials. However, this precisely fulfils its function by keeping bicycles permanently strong and safe at the right height.