Solution
Years before the project, several Demag cranes were retrofitted with our energy chains, which are still in operation today. Downtime due to maintenance, Corus Rail says, has never been necessary. In contrast to the festoonings, regular visual inspections are now sufficient for the energy chain solution.
For the modernisation of the cranes in the current project
energy chains of the type E4/4 HD were fitted. In the pin-bore connections of this chain, the load-bearing surfaces have been increased by 120% compared to the previous model. Due to the considerably larger wear surfaces, the strength and service life of the energy chain have been further increased. This predestines the E4/4 HD for high loads in dirty environments on long travels at high speeds.
The new energy supply system was supplied as a
fully pre-assembled complete readychain package, and installed immediately on site by our UK team. The benefit: reduced costs for installation time, hardly any loss of valuable production time.
The chains are filled with
chainflex cables (CF310 motor cables, CF9 and CF10 control cables and CFLG FO cables) for outdoor use. Highly abrasion-resistant TPE jackets make the cables ideal for harsh environments. They are UV-resistant, can be used at high temperatures between -35°C and +100°C, and have a very high media resistance to coolants and lubricants. The 90% optical coverage of the shielded cables with a coordinated braiding angle increases the requirement for high EMC safety.