No more lubricating: for balers, loader wagons, manure spreaders, tippers, and field sprayers, ROCKINGER Agriculture GmbH is developing a ball coupling called KS80 using a high-performance plastic from the iglidur series that igus developed specifically for the company. The coupling consists of a coupling ball and claw installed in the height adjustment system.
As usual, the coupling claw is positioned on the ball head from above. It is secured against inadvertent decoupling with a hold-down device and creates a clearance-free connection. What is special about this coupling becomes apparent only upon inspection of the inside of the coupling claw. It contains a wear insert made of high-performance plastic, the wear resistance of which has been proven in laboratory tests.
In a fatigue test, the inserts survived two million load changes- with a support load of 4.5t. ROCKINGER Agriculture GmbH calculates that if a third of the tractors in Germany were equipped with a KS80 and wear insert, around 8,300 couplings would require no lubrication. Eight tons of grease could be saved each year.
More about customised components made of iglidur materials