Option 1
as a sacrificial cable
In this option, space is still needed to route an additional cable in the e-chain® because the CF.Q is routed as a "sacrificial cable" in the e-chain®.
All cores of the cable are "connected in series" and connected to the measuring input of the module.
Advantage: All cores are measured, which means that there is no need to select the most frequently used cores.
Disadvantage: Regardless of the production batch and the assembly method, even cables from the same production batch can achieve different service life durations.
Option 2
unused cores of a cable
In a monitored cable, two unused cores are defined as measuring cores and, if necessary, routed to the measuring connections of the CF.QA module by means of a shielded extension cable.
This often requires a modification of the connector assembly, as the two cores must be led out of the connector on the distributor side at the cable entry.
Advantage: The cable actually used by the customer is monitored
Disadvantage: The original cable often has to be replaced by a variant with two additional cores, which usually increases the cable diameter, and the apparently "weakest" cores should be chosen.