Present worldwide
Since 2011, the Feucht site has been part of the AGCO Group, which is one of the three largest agricultural machinery manufacturers in the world with around 20,000 employees, a turnover of around 7.5 billion US dollars and strong brands such as Fendt, Massey Ferguson and Fella. However, the tradition of agricultural engineering at the site is much older, precisely 100 years old: In 1918, the "Bayerische Eggenfabrik AG" was founded in Feucht and in 1921 the Fella brand was launched. Today, being part of a global group enables the company to create the conditions for international presence: from Feucht, the machines are delivered to around 120 countries.
Ideal bearing for extreme conditions
An important design element, especially in the larger mower units, is the movable mounting of the mowing bars on the base frame. The beams are folded up in the transport position, on site they are hydraulically swivelled into the horizontal position. The bearing is supported by igus bearing bushings made of iglidur high-performance plastics with incorporated lubricants.
The fact that plastic is used at this critical point at least needs an explanation. Because the forces and conditions to which the bearings are exposed are more than unfavourable. The tractor travels over uneven terrain at speeds of up to 15km/h. The mowing tools encounter stones and other obstacles, which causes a heavy impact load on the bearings each time. Also the temperatures can be quite extreme and since mowing is always carried out when dry, high levels of dust and dirt are part of the environmental conditions. Added to this is the weight of the sickle bar, which also acts on the bearings.
Plastic instead of brass bearings
All in all, one can imagine the bearing application as a continuous load test - which the igus bearings easily master over a very long period. "We have been using igus bearing bushings for years, have built thousands of machines since then and are very satisfied with this solution," explains Jochen Gnann.
There were several reasons for the substitution of the previously used brass bearings at the time: "A metal-to-metal contact among moving components is always difficult. In addition, we were looking for a bearing that did not require lubricants, because the farmer did not want to lubricate and in the very dusty environment this would quickly lead to strong dirt adhesion. " Apart from the technology, the economic efficiency also speaks for the iglidur bearing bushings: The market for agricultural machines is very price-sensitive, and the plastic bearings are more cost-effective than brass bushings.
Small component - big effect
AGCO Feucht GmbH uses iglidur plain bearings from igus not only at the critical connection of the base frame and cutter bar, but also - mostly in smaller installation sizes - at various other bearing points of mowers, hay turners and rakes. There is a simple reason why the picture shows greased bearings. The grease is only used by employees in production to facilitate the insertion of the shaft. During operation, the bearing points do not require any lubrication at all, over many years of rough use on the turf. Jochen Gnann concludes: "Small component - big effect. “