Solution
Due to the repeated problems and increased downtimes of the entire plant, the operator made more enquiries for a suitable solution. In spring 2019, a project to overhaul the cable guidance system was finally launched by the operator together with an igus project team. Close contact, which lasted for several months, covered the entire process from project design to the final installation of the new cable guide. The core of the new solution is a huge energy chain with a travel of 670m. This has set the current world record, as it is the second plastic energy chain worldwide with this travel length.
Since such a superlative solution can of course also lead to uncertainties, the proposed chain - an
E4/4 type 5050RHD roller energy chain sample - was extensively tested in advance in our in-house laboratory.
The cables are guided safely inside the chain and are better protected against external influences. Our
chainflex cables, designed for moving applications and designed in conjunction with our energy chains, were also used in the new cable guide. In order to provide additional planning security for these dimensions, the entire cable guide is supplemented by smart plastics, i.e. intelligent sensors in combination with energy chains.
So-called
iSense modules ensure continuous condition monitoring by sensors measuring the prevailing push/pull forces along the chain. These data are evaluated via a module in the switch cabinet and can perform actions, such as shutting down the system, if a limit value is exceeded. Damage to the cable guide can thus be prevented before it occurs.
Overall, the interplay of energy chain, cables and sensors has resulted in a solution that was able to make a major leap forward in terms of plant availability, durability and safety during operation. The plastic energy chain saves weight, simplifies cable guidance and saves the operator high maintenance effort and costs.