Solution
To supply energy and data, we offered the customer
readychain - a complete energy chain system, which is ready to connect. While machine experts previously had to put together individual chain links themselves and thread cables laboriously, this work is a thing of the past with our harnessed system. Altogether, the manufacturer can save about 80% of working time. The energy supply system contains servo and encoder cables from the
chainflex cable product range as well as hydraulics and coolant hoses. All components are already harnessed with the right plug-in connectors. The cables and hoses are specifically designed for use in the energy chain and are tested under real-world conditions in our in-house 3,800 square metre laboratory. Customers are offered a guarantee on the complete system.
DVS Universal Grinding GmbH currently offers the machine series in two sizes. The UGrind 800 for workpieces with centre distances of not more than 1,200 millimetres and the UGrind 1500 for sizes of up to 1,800 millimetres. For the larger, functionally identical machine, the chain system merely had to be extended by three chain links. The
readychain system installed in the machines today consists of three harnessed energy chains. In the Z-axis, two lightweight
E4.1L energy chains (E4.38L series) supply the multifunction turret with the appropriate cables and hoses. They can be assembled quickly and are cost-effective. An
E4/light energy chain (14240 series), which is also very lightweight and cost-effective, is used in the X-axis. Reduced side link thickness and a thinner crossbar gives the chain more room in its interior for cables. DVS Universal Grinding GmbH is also convinced of the quality of the energy chain systems. The first machine with the readychain has been in use for a customer in high-volume production 24 hours a day, six days a week for more than 18 months, without any problems.