Solution
Since conventional cables do not meet the ZEMA requirements for service life, the company basically uses
chainflex cables from igus for remote controls. The chainflex cables are designed quite differently from those for static applications: the principle of cores wound in bundles ensures that the tensile and compressive forces acting on the individual cores during movement are balanced. This creates an essential prerequisite for a long service life in moving applications - without broken cores and corkscrews. The high-quality materials and the special extrusion process prevent further causes of failure, for example jacket abrasion and insulation damage.
Twistable chainflex cables of the CFROBOT9 series are used in the ZEMA machines. The cables achieve a long service life in the field and also facilitate the handling of the remote control because they are more flexible and therefore more mobile.
ZEMA obtains the cable sets as fully harnessed energy supply systems (
readycable). This has the advantage that the customer saves a lot of time and does not have to keep plug-in connectors or other accessories ready. And despite the commitment to one standard, Josef Zeyer GmbH remains flexible because the harnessed cables can be ordered in different lengths.