Durable premium components from Cologne
The manufacturer advertises the use of premium components, especially for the newly developed pedals from Crankbrothers. This also includes iglidur plain bearings, which are optimised for friction and wear. A long service life combined with a very lightweight feature are important criteria in the bicycle industry. Since our plain bearings operate dry, no dirt can stick to them. As a result, the bearing points remain smooth even in the most adverse conditions. "In addition, there are very large impact loads in the open country which the bearings have to withstand," explains René Achnitz, head of the iglidur plain bearings division at igus. “Our solutions can easily keep up with the specifications of metallic alternatives.” However, the lightweight feature is at least as important when cycling as the functionality of bearing points, as every gram to be moved requires additional force from the rider.