Problem
The parcel locker system is used by the general public in a variety of places, e.g. outdoors, lobbies, offices, etc. Therefore, the challenge was to enable the most instinctive use possible, so that the product fits perfectly into the user's path. In addition, a very high service rate and thus maximum ease of maintenance had to be ensured. The problems were: the simplicity of implementation, the simplicity of use over time (no grease and oil, no wear), the quality of movement (no noise, fluid) and a certain mechanical resistance (allowable loads largely dimensioned in relation to the system).
Solution
The products from igus® are very suitable in this sense, as they are free of grease and oil. In addition, maintenance requires only periodic inspection. The dryspin® lead screws are installed in the SAS opening and module soldering. They provide less noise, less regular maintenance and reliability. The iglidur® polymer plain bearings are used in electromagnetic guidance and enable improved guidance and less friction. The drylin® linear guide is also installed in the SAS opening and also in the vertically motorised axis. There they can prevent noise and maintenance, are easily mounted and could convince with their size.