e-chain® reel

Mobile socket for 8/10kV medium voltage cables

Clean energy supply for ships

The igus e-chain reel is a motor-driven, reelable energy chain system equipped with a special chain with roller inserts that can be used to flexibly position the socket within a range of up to 100m. This allows more ships to be supplied than permanently installed systems can manage.

igus shore power supply solutions, such as the e-chain reel, use generators to provide ships with power while they are in port so that power need not be produced on the ship. This sustainably protects the environment and the health of those in the port area. Powering an entire ship is a major challenge. In addition to the technical challenges of the power supply system (such as the right voltage and frequency), the place where the cables coming from the ship have to be connected also changes from ship to ship.
Send a query about an e-chain reel now
e-chain reel
e-chain reel
Tech up

Tech up

  • Move the socket trolley to the connection point for flexible shore power connection
Cost down

Cost down

  • Long cable service life thanks to guidance with a special chain with roller inserts
Proof

Proof

  • Arc fault protection thanks to a tested outlet box
Recycling

Sustainability

  • No harmful emissions: shore power instead of vessel engines running
  • Have your energy chain recycled at the end of its life cycle with the igus chainge recycling program. No matter what manufacturer. You will receive a voucher

You might also be interested in

Energy chains shop

Energy chains shop A shop with more than 100,000 products for unsupported, gliding, hanging, and standing applications.

Energy chain configurator

Energy chain configurator Assemble your individual energy chain system in just a few steps.

Energy chain recycling

Chainge program for energy chains Have energy chains recycled instead of throwing them away.