Solution
In order to simplify the process for Bluhm and shorten assembly times, the customer was promptly offered a ready-to-install format adjustment.
The
drylin® linear guides used not only give maximum flexibility to the Tamper Evident with its adjustment unit when customising the labeller, they are also resistant to dust and dirt, making the labeller also suitable for harsh environments. In addition, the linear guides operate without additional lubrication, since their sliding elements contain incorporated lubricants. This not only saves the user maintenance time later on, but also costs for maintenance and lubricants.
The long service life of drylin® linear guides enables Bluhm Systeme GmbH to supply its customers with a top quality product. With the repeatability, precision and speed of the drylin® components, the batch change time of the Tamper Evident could be reduced. The labeller can apply 500 seal labels per minute. Here, every second that you can save on the adjustment pays off. This is why the complete automation of label changeover and format setting is a topic that is consistently pursued at Bluhm. It saves additional time and reduces sources of error. Further co-operation is already planned for the future, as demand for the machines continues to grow.