Solution
In the case of linear systems, we are already a long-standing partner of Indspect. The
drylin® SHT linear modules that are used offer resistance to corrosion and chemicals as well as freedom from maintenance. They are easy to clean and have low moisture absorption. In addition, they are light and do not require additional lubrication. The lead screw linear units are recommended for aggressive environments. A stainless steel version with corrosion-free steel components also meets the highest demands of the food industry.
The manufacturer already knew the products from previous collaborations. He is thereby able to meet all hygiene requirements and keep the aging process low. This enables customers to use the system for many years.
The camera and lighting also move along in the adjustments in the Indspect devices. The drylin® SHT was used here almost from the beginning. An appropriate energy chain was included a little later. In large systems where many cameras work, it secures the cables and therefore the operation. The E14 series
easy chain® energy chain is easy to fill quickly along the outer radius. A "push-button design" safely holds the chain links together. A small pitch ensures quiet, smooth operation.
To date, there have been no known complaints about the systems, and it only returns to the manufacturer if something is rebuilt or a part is added. Maintenance work is also not necessary thanks to the lubrication-free nature of the linear systems. In this way, the high expectations of the food industry for the linear systems could be met right from the start. This also applies if entire units - such as linear systems - are on the order form. Extensive assembly work is completely eliminated.