Problem
Components in pallet production systems are exposed to special loads. These include wood chips and dust, moisture and resin. In addition, the dynamics of many drives are high, with 50,000 strokes per day. This applies, for example, to the handling units of the nailing station. The linear guides must be able to withstand alternating loads in a dusty environment as the moving ends attached to the axes move up and down when they remove a board from the storage. Added to this are the continuous vibrations caused by nailing.
The designers were dissatisfied with conventional bearings, such as ball bearings and recirculating ball bearing guides, as they did not help achieve convincing service lives.
Solution
After tests with different bearing types, drylin linear bearings proved to be the best solution. They allow for the longest service life, which is around three months. At first, that doesn't seem like much. However, if you multiply 50,000 strokes by 90 days, this results in 4.5 million working cycles and that in combination with dirt, high dynamics and alternating loads. The linear housings are equipped with liners made of wear-resistant iglidur J plastic and, thanks to the incorporated solid lubricants, do not require any external lubrication. As a result, no dirt sticks to them, maintenance is superfluous and the axes are guided with extreme precision.
Krenzer is so convinced by the dry-running bearings that they are not only used on the removal units for the cover boards from the storage, but also for the feeding and exact positioning of the cover boards.