Cocktails by touchpad
The way in which the "CocktailAvenue" – this is what the system is called – works is easy to explain. The user chooses a cocktail on the touchpad and places a glass in the holder, which is mounted on a linear axis and travels below one of nine bottles. A lifting pin moves upwards out of the holder, in the process opening a dispensing unit that fills the desired amount of the liquid into the glass. The process is then repeated, depending on the number of ingredients in the cocktail. The linear unit then moves to a separate station where the glass if filled with one or several juices - This completes the cocktail mixing process.
The entire process can be seen, as can the drive. A real "eye-catcher", not only for industrial automation technology trade fairs but also for other events, private parties and, of course, in the area of gastronomy; after all, cocktails are "in".
The idea of the "cocktail machine" comes from Robert Becsei in Friedrichshafen. He established the start-up company AlphaInvent and is now working with his business partner Wilhelm Merker on further development of the business idea, which catering companies and bar owners, for example, are currently greatly interested in. This is not surprising. Robert Becsei: "Watching the machine mix a cocktail generates a considerable "wow" effect. “