Solution
Today, plastic plain bearings play an important role for the movements of the grippers. Specifically,
drylin R linear bushings of type RJMP-01-25 are used here. They were favoured by Krones because they are made of plastic and are therefore lightweight, cost-effective and yet very tough. This has been very well demonstrated in practice: Krones has not yet had any complaints about the resistant bearings. They are robust against shocks or dirt and also withstand strong vibrations or extreme weather conditions. Here again, it is the small refinements that count, such as the special segmented design of the bearings. This special feature proves its worth in dusty environments. This is where the compressed dust molecules normally accumulate on the guide shaft. As the dust layer increases day by day, the diameter of the shaft increases. As a result, the traversing movement becomes increasingly sluggish due to the strong friction.
Everything runs better in the plain bearing with the slots. There, the dust does not settle in the bearing, but is literally carried through the bearing without any significant changes in friction and wear behaviour.
The Krones gripper specialists, on the other hand, have had different experiences with the previously used recirculating ball bearings. Even a collision could destroy such bearings. The balls are often pressed into the shaft.
But 'conventional' packaging grippers from Krones also benefit from the plain bearings during operation. Because the plastic plain bearings fit perfectly into Krones' modular gripper system.