Solution
Walterwerk Kiel GmbH & Co. KG pursued various approaches as a solution for format adjustment and finally decided on a simple as well as reliable system solution that can be adjusted manually by the user. To be more precise, the special machine constructor has been using lubrication-free plain bearing technology in their modular baking systems for format adjustment for many years now. The
drylin lead screw unit used is maintenance-free, cost-effective and versatile. Plain bearings made of high-performance plastics for the food and packaging environment are FDA-compliant depending on the choice of material. Product contamination by an additional active lubricant is excluded. Friction and wear have been optimised due to their tribological properties, which has a positive effect on the operating times of the machine. Even regular cleaning with aggressive media does not pose any problems for them.
The special machine manufacturer obtained the complete lead screw unit harnessed as a system. Doing this has been agreeable not only for the technical parameters that are exclusively designed for the local requirements, but also for the business operation.
For example, in a wafer baking system being delivered to Korea, two parallel systems had to be simultaneously adjustable over a length of almost one metre. The two lead screws are coupled via a helical bevel gear wheel on one side. Due to the low loads a shaft construction for support could be dispensed with. The aluminium guide tube guides the inner-lying stainless steel lead screw. The material combination withstands the adverse ambient conditions. There is also a position indicator and a hand wheel. The whole system is maintenance-free. And due to the absence of lubrication, contact with food is safe.