Solution
Strong energy chains are especially well suited to the high loads involved in supplying engines on special vessels. In this case, our
E4.1 series energy chains, characterised by a high level of robustness combined with compact dimensions, are used. In the case of the seismic survey vessel, interlocking energy chains were used to save installation space. For additional strength, they are designed as multiband chains, meaning that they have additional chain bands with which the system can safely move the high cable weights over the long term. And in order to minimise the load on the guided cables given the high forces, special
strain relief elements were integrated.
Since we develop our
chainflex cables specifically for moving applications, special cables in energy chains were an obvious solution. They accept the low bend radii resulting from the tight spaces in the drives.