Solution
Because of the welding work on the platform, only closed cable guidance was possible. More precisely, work surface movement is supported by an
E4.1 series energy chain in a
fully enclosed e-tube system design.
Special feature: The lightweight plastic energy chain easily withstands the high temperatures of fast flying swarf, and the cables are always protected. The system's particularly good gliding properties also ensure smooth movement. This advantage is particularly noticeable on the long travels during longitudinal movement of cranes in the ship's interior.