Solution
Beyer works with a high level of vertical integration and takes great care in the optimal selection of purchased components - for example, the energy chains. Today,
energy chains of the E4.1 series are compelling here due to their higher torsional stability compared to the chains previously used by Beyer. For this reason, the manufacturer used the cable guidance (in version E4.28) throughout the system series and sizes.
The E4.1L series is also convincing in terms of noise reduction. The individual plates on the chain links glide smoothly into one another during the movement, because the wedge-shaped radius stop is slightly bevelled. This dampens the noise while stopping as well as when rolling on hard ground. Vibrations are also reduced, which further increases the service life.
In addition, the E4.1L can be opened and filled very easily from both sides. This saves time especially when installing on the machine.
In some applications, Beyer also uses the closed version of the energy chain as energy tube R4.1L - and always when there is a risk of glass breakage in the work area.
Finally, the machine specialist also relies on the
chainflex cable systems specially developed for moving applications. In addition to energy and signal cables, up to four pneumatic hoses with diameters of 12 millimetres are carried along, which "work" during pressure changes and introduce additional loads into the energy supply system. The E4.1L copes very well with these loads.