Solution
The sophisticated solution: A sliding element specially developed for KHS, which is not flat on the inside of the shaft, but has a fluted structure. The advantage is that during cleaning, the interior of the bearing is not left out, and hygiene standards rise. The new
drylin JUM-01-30 type liners have a burl-like structure on the outside. Here, too, water can simply flow through and thus reach even the smallest dirt particle.
The bearings made of the standard iglidur J material naturally also work with incorporated lubricant to prevent product contamination by oil or grease.
And the tests prove the effectiveness of the special bearings. Due to the special surface structure on the inside and outside of the bearings, the highest hygiene requirements are met. Germ tests by KHS prove this.