Solution
From day one, high-performance energy supply systems and cables from our energy chain range are used in the Omnicell systems. Specifically, e-chains from the
E2/000 series are used, which can be opened from the inside and the outside, and are characterised by easy and versatile assembly.
Usually, between two and five completely harnessed energy chain systems are used, which are called "readychains". They combine robustness and abrasion resistance and operate quietly with low vibration. Moreover, they need little installation space due to the small bend radii. This is very important in order to be able to use the space available in a medicine storage space most effectively. Because of the very small chain link pitch and the resulting reduced polygon effect, there are hardly any vibrations or shocks. This means that the chemist's customers barely notice the background picking processes that provide the medicine as if by magic.
They contribute to the good technical data of the systems while minimising the installation effort.
But we also provide the cables ourselves. At Omnicell, for example, functionally reliable servo, bus, control and pneumatic cables from the
chainflex range ensure the required performance data for fast picking of the medication packaging.